Populate Customer Table
To implement Responder, a Database Administrator will need to populate the customer table in the Responder database.
Some of the fields in the Responder tables utilize domains. Domains may be edited in the DatabaseSchemaConfig.xml file.
The customer table must be populated to use Responder. The Responder database consists of additional Responder tables which may be modified to customize Responder Explorer, as well as history tables and archive tables.
RX_CUSTOMERS
Populate this table with your existing CIS data. The Account field is the primary key for the table and must be restricted to NOT allow duplicates. Duplicate account numbers will cause errors in Responder and prevent the user from accessing the Edit Incident form.
|
Field Name |
Description |
|---|---|
|
ACCOUNT |
The customer's account number. This field is the primary key for the table. Duplicate account numbers may NOT be allowed. |
|
ACCOUNT_TYPE |
Indicates the type of account. Uses the Account_type domain. |
|
METER |
The customer's meter number. |
|
FIRSTNAME |
The customer's first name. |
|
LASTNAME |
The customer's last name. |
|
STREET |
The customer's street address. |
|
CITY |
The customer's city. |
|
STATE |
The customer's state. |
|
POSTAL_CODE |
The customer's zip code. |
|
TELEPHONE |
The customer's telephone number. The area code of a phone number may not begin with a 1 or 0. |
|
TELEPHONE2 |
An alternate telephone number for the customer. The area code of a phone number may not begin with a 1 or 0. |
|
TELEPHONE3 |
An alternate telephone number for the customer. The area code of a phone number may not begin with a 1 or 0. |
|
TELEPHONE4 |
An alternate telephone number for the customer. The area code of a phone number may not begin with a 1 or 0. |
|
CALLBACK_NUMBER |
Preferred number for contacting the customer. The area code of a phone number may not begin with a 1 or 0. |
|
DEVICE_OID |
The object ID of the device to which the customer is associated (e.g., service point or transformer). This field links to the OID field in your geodatabase. |
|
DEVICE_FCID |
The feature class ID of the device to which the customer is associated (e.g., service point or transformer). This field utilizes the DEVICE_FCID domain. |
|
CONNECT_STATUS |
Indicates the status of the user's connection (connected/disconnected). This field uses the CONNECT_STATUS domain. |
|
CRITICAL |
Indicates if the customer site is critical. This field uses the CRITICAL_TYPE domain. |
|
PRIORITY |
Indicates if the customer site is priority. This field uses the PRIORITY domain. |
|
TIME_DISCONNECT |
Indicates the time the customer was disconnected. |
|
TIME_RECONNECT |
Indicates the time the customer's power was reconnected. |
|
USER_CREATED |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who created the record. |
|
USER_UPDATED |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record. |
|
REGION |
Indicates the region in which the customer resides. This field uses the REGION domain. |
|
COUNTY |
Indicates the county in which the customer resides. |
|
FEEDER_ID |
The ID of the feeder to which the customer is attached. |
The remaining tables in the Responder database are populated by Responder.