Callback List
When incidents are edited, the Callback List may be impacted, depending on the scenarios activated. The tables below describe how specific changes to an incident may affect the Callback List.
All Scenarios
This table displays the incident edits that affect the callback list regardless of the scenarios activated.
Operation Performed on Incident |
How Callback List is Affected |
---|---|
Cancel Incident |
Customer(s) associated with incident are removed |
Reassign calls associated with an incident |
Updates the incident ID associated with customer on callback list |
Save As New Incident |
Changes incident ID |
Incident Created
This table displays the incident edits that affect the callback list when the IncidentCreated scenario (i.e., the CallbackOnPowerOut event) is enabled.
Operation Performed on Incident |
How Callback List is Affected |
---|---|
Add Device to Incident |
Customers added to the list |
Consolidate Incidents |
Change incident ID and adds new customers |
Move Upstream |
Customers added to the list |
Change Device |
Customers added to the list for new device; customers removed from list for original device |
Incident Restored
This table displays the incident edits that affect the callback list when the IncidentRestored scenario (i.e., CallbackOnPowerRestored event) is enabled.
Operation Performed on Incident |
How Callback List is Affected |
---|---|
Change Device |
Customers added to the list for new device; customers removed from list for original device |
Remove Device |
Customers removed from list |