RX_INC_DEV_ASSIGNMENTS

Field Name

Description

INCIDENT_DEVICE_ID

The ID of the device. This field serves as a foreign key to the RX_INCIDENT_DEVICES.

CREW_ASSIGNMENT_ID

The unique identifier assigned to each crew assignment. This field corresponds with the ID field in the RX_CREW_ASSIGNMENTS table.

USER_CREATED

The name of the user who created the record. This field is populated automatically by Responder.

USER_UPDATED

The name of the user who updated the record. This field is populated automatically by Responder.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?