Exclude Planned Switching Values from the Dashboard

You can exclude customer counts associated with planned switching from the elements visible on the Dashboard.

To remove planned switching values from the Dashboard, look for the following XML in Web.config. By default, this file is installed here: C:\Inetpub\wwwroot\Responder.

    <add key="dashboard.excludePlannedSwitching" value="false" />

Set the "value" to true. The following dashboard elements will no longer include planned switching customer counts:

Geospatial Tab:

  • Customers Interrupted

  • Interruption Count

Analytical Tab:

  • Customer Status (All Sub-Elements)

  • Interruption Status (All Sub-Elements)

Tabular Tab:

  • Customer Status (All Sub-Elements)

  • Interruption Status (All Sub-Elements)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?