Create Historical Database

TroubleMaker requires a database from which it submits customer calls to Responder. Use the sample database called TroubleMakerData.mdb, which is installed with TroubleMaker in Program Files\Miner and Miner\Responder\TroubleMaker\.

TroubleMakerData.mdb contains all of the fields required by TroubleMaker to execute scenarios. This database contains the tables listed on this page. These tables along with their fields are described below.

TIP: You can also create new databases directly from the Generate TM Data From Archive tab.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?