Responder Database Tables
The tables on this page may be modified to customize Responder Explorer. The field data is populated by Responder. Modifications to these tables are not required to configure Responder.
Some of the fields in the Responder tables utilize domains. Domains may be edited in the DatabaseSchemaConfig.xml file.
Information on FCID fields can be found in your geodatabase in the GDB_ITEMS and GDB_ITEMTYPES tables.
You can check the data architecture of each Responder table (i.e., field data type, field length) by viewing the SQL implementation scripts in your Miner and Miner\Responder\Developer Resources\Implementation Scripts directory.
The following tables are for internal use only. Do not modify the data in these tables.
-
RX_ELEMENT_LOCKS
-
RX_EVENTS_FEEDERLOCK
-
RX_PENDING_ELEMENT_LOCKS
-
RX_PERMISSION
-
RX_PROBABLE_STATE_CANDIDATE
-
RX_ROLE
-
RX_ROLE_TASKS
-
RX_TASK
-
RX_TASK_PERMISSIONS
-
RX_USER_MEMBERSHIP
-
RX_USER_ROLES
-
RX_USERS
-
RX_XLOCK