RX_SW_OR_FEATURES_ARCHIVE
Field Name |
Description |
---|---|
SW_OR_FEATURES_ID |
The ID associated with the switching order feature. |
INCIDENT_ID |
The ID associated with the incident resulting from the call. This field corresponds with the ID field in the RX_INCIDENTS table. |
OID |
Object ID of the feature associated with the tag. |
FCID |
Feature class ID of the feature associated with the tag. |
SUBID |
The unique ID of each segment of a complex edge. |
X |
The x-coordinate of the incident device. |
Y |
The y-coordinate of the incident device. |
USER_CREATED |
The name of the user who created the record. This field is populated automatically by Responder. |
USER_UPDATED |
The name of the user who updated the record. This field is populated automatically by Responder. |
FACILITY_ID |
The Facility ID of the incident device as defined in the geodatabase. |
REGION |
The region in which the feature exists. This field uses the REGION domain. |
SUBSTATION |
The substation that feeds the incident device. |
COMMENTS |
Notes from the operator or dispatcher. |
ENABLED |
Not used. |
SUBTYPE |
The subtype of the device. |
FEEDER_ID |
The Feeder ID of the feature. |
PHASE_DESIGNATION |
The phase designation of the device. |
OPERATING_VOLTAGE |
The operating voltage of the device. |
NAME |
The name assigned to the device. |
CHANGE_DATE |
The time and date an operation was performed on the record. |
OPERATION |
The operation (e.g., insert, delete, update) performed on the record. |
USER_UPDATED_ARCH |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record. |
SW_ORDER_REQUEST_ID |
The unique ID assigned to the switching order request. |
AFFECTS_ENERGIZATION |
Indicates whether the feature participates in the geometric network (electric device) or not (location feature). |
FEATURE_CLASS_NAME |
The name of the Feature Class on which the incident occurred, as it was configured/named when the Incident was archived. |