RX_SW_OR_AFFECTED_LOADPOINTS

Field Name

Description

OID

Object ID of the feature associated with the loadpoint.

FCID

Feature class ID of the feature associated with the tag.

SW_ORDER_REQUEST_ID

The unique ID that identifies the switching order request to which the loadpoint was assigned.

USER_CREATED

The name of the user who created the record. This field is populated automatically by Responder.

USER_UPDATED

The name of the user who updated the record. This field is populated automatically by Responder.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?