Clustering Server 2008 R2
Server clustering is not a required part of the Responder implementation. If you choose to implement server clustering, server clustering provides failover support for the Responder services and message queues. If one Responder server should fail, its workload is shifted to another server in the cluster without impacting Responder users.
The Responder server is installed as a virtual server. This enables the Responder services to failover to a different server should the physical server fail.
To support scaling-out across multiple servers, Responder uses a component called a Message Router to route messages from the client facing queues to the back-end Responder services (such as, Data Services and Prediction Services). The image below shows the Message Router component in a group (to allow for failover) forwarding messages to additional server machines that participate as active nodes in an active/active server cluster. If an active node failover occurs (in the responder business services cluster), the active node resources are transferred to another node.
Only one Line Display Services per organization can be running at a time.