Limit Number of Customers Returned by Search

This setting allows you to determine the maximum number of customers returned when the user performs a search using the Find Incident For Customer tool. The default setting is 100.

If the number of records matching the search criteria exceeds the CustomerListSizeLimit value, the user is prompted to narrow the search.

To modify this setting, open the Miner.Responder.Explorer.exe.config file installed in: Program Files\Miner and Miner\Responder\Client.

Look for the following XML:

               <add key="CustomerListSizeLimit" value="100"/>

Set the value attribute to the maximum number of records that can be returned. Save and close Miner.Responder.Explorer.exe.config.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?