RX_INCIDENT_FEATURES
Field Name |
Description |
---|---|
OID |
Object ID of the feature associated with the incident. |
FCID |
Feature class ID of the feature associated with the incident. |
SUBID |
The unique ID of each segment of a complex edge. |
X |
The x-coordinate of the incident feature. |
Y |
The y-coordinate of the incident feature. |
INCIDENT_ID |
The ID associated with the incident. This field acts as a foreign key to the RX_INCIDENTS table. |
TIME_REPORTED |
Time that the feature was reported out. |
CONFIRMED |
Indicates whether the feature has been confirmed out. This field uses the CONFIRMED domain. |
FACILITY_ID |
The Facility ID of the incident feature as defined in the geodatabase. |
USER_CREATED |
The name of the user who created the record. This field is populated automatically by Responder. |
USER_UPDATED |
The name of the user who updated the record. This field is populated automatically by Responder. |
REMARKS |
Notes from the operator or dispatcher. |
REGION |
The region in which the device resides. This field uses the REGION domain. |
CANCEL_REASON |
Reason the feature was cancelled. |