RX_JUMPER_STEPS_ARCHIVE

Field Name

Description

JUMPER_STEP_ID

The ID associated with the Jumper.

OPERATION_ID

The ID field from RX_OPERATIONS (foreign key).

TRACE_WEIGHT

Field containing information used by Feeder manager to utilize the Jumper when tracing the network.

EDGE1_FCID

Feature class ID of the first initial conductor clicked to place the Jumper.

EDGE1_OID

The object ID of the first initial conductor clicked to place the Jumper. This field links to the OID field in your geodatabase.

EDGE1_SUBID

The subnetwork ID of the Edge that represents the initial snap point of a Jumper.

EDGE2_FCID

Feature class ID of the second and final conductor clicked to place the Jumper.

EDGE2_OID

The object ID of the second and final conductor clicked to place the Jumper. This field links to the OID field in your geodatabase.

EDGE2_SUBID

The subnetwork ID of the Edge that represents the terminating snap point of a Jumper.

DISPATCHED_BY_NAME

The name of the dispatcher who executed the Jumper.

Points

This field represents all the points on the map a user clicked when creating a Jumper.

CHANGE_DATE

The time and date an operation was performed on the record.

OPERATION

The operation (e.g., insert, delete, update) performed on the record.

JUMPER_GUID

The GUID assigned to the Jumper.

STEP_TYPE

Field that differentiates between steps that Place or Remove Jumpers.

JUMPER_NAME

The name assigned to your Jumper.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?