Line Display Services

Line Display Services is responsible for including the line energization state on the map. Use the Line Display Services tab to configure, manage, and execute a single Line Display Services. One Line Display Services instance must be running to use the console which means the Count field must contain a one.

NOTE: Only one Line Display Services per organization can be running at a time.

IMPORTANT: For Oracle users: When installing the Oracle Client, ensure the Oracle Services for Microsoft Transaction Server component name is selected. Existing Oracle users, modify your Oracle client installation to include this component. This component is required for the Line Display Service to run correctly, even for local installations.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?