Configuration File Updates - 9.1.2 SP1

This table indicates which Responder configuration files are upgraded for the 9.1.2 SP1 release. Note that Version Change indicates that only the file-version number has been updated in the configuration file. It is important that this update be made. Upgrades for subsequent releases will fail if the file-version number is not accurate.

  • New: This file is new for this release.

  • Removed: This file does not exist for this release.

  • Upgrade: This file has changed for this release. The existing file must be upgraded.

  • Version Change: This file has not changed for this release. The existing file must be upgraded with file-version number only.

Component

Configuration File

Update

client

Miner.Responder.ArchiveExplorer.exe.config

Upgrade

client

Miner.Responder.Explorer.exe.config

Upgrade

TroubleMaker

Miner.Responder.TroubleMaker.exe.config

New

TroubleMaker

TroubleMakerConsole.exe.config

Removed

web

Web.config

Version Change

web

WebConfig.xml

Version Change

web

WebRemoting.config

Version Change

server

Web.config

Version Change

server

WebRemoting.config

Version Change

server

ArchiveQueriesConfig.xml

Upgrade

server

ArchiveSchemaConfig.xml

Version Change

server

ArchiveStylesConfig.xml

Upgrade

server

ArchiveSubmitRulesConfig.xml

Version Change

server

ControlStylesConfig.xml

Upgrade

server

DatabaseSchemaConfig.xml

Upgrade

server

ExplorerRulesConfig.xml

Upgrade

server

security.xml

Version Change

server

SubmitRulesConfig.xml

Upgrade

server

Miner.Responder.ArchiveServices.exe.config

Upgrade

server

Miner.Responder.DataServices.exe.config

Upgrade

server

Miner.Responder.PredictionServices.exe.config

Upgrade

server

Miner.Responder.WindowsService.exe.config

Upgrade

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?