RX_INC_DEVICE_STEPS_HISTORY
Field Name |
Description |
---|---|
OPERATION_ID |
This field corresponds to the ID field in the RX_OPERATIONS table. |
EXPECTED_STATUS |
The expected or normal status of the device (open, closed). |
PLANNED_STATUS |
The planned status of the device (e.g, Open, Closed). |
PLANNED_CUSTOMER_COUNT |
The number of customers affected by a planned step. This value indicates a net change in the number of energized customers. It will be either a positive number (power restored to customers) or negative number (customers losing power). |
PLANNED_CRITICAL_COUNT |
The number of critical customers affected by a planned step. This value indicates a net change in the number of energized customers. It will be either a positive number (power restored to customers) or negative number (customers losing power). |
PLANNED_CONNECTED_LOAD |
Amount (in kVA) by which the total system connected load will change due to the planned step. |
EXECUTED_CUSTOMER_COUNT |
The number of customers affected by an executed step. This value indicates a net change in the number of energized customers. It will be either a positive number (power restored to customers) or negative number (customers losing power). |
EXECUTED_CRITICAL_COUNT |
The number of critical customers affected by an executed step. This value indicates a net change in the number of energized customers. It will be either a positive number (power restored to customers) or negative number (customers losing power). |
EXECUTED_CONNECTED_LOAD |
Amount (in kVA) by which the total system connected load will change due to the executed step. |
USER_CREATED |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who created the record. |
USER_UPDATED |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record. |
CHANGE_DATE |
The date an operation was performed on the incident record. |
OPERATION |
The operation (e.g., insert, delete, update) performed on the incident record. |
ACTUAL_STATUS |
The current actual status of the device (open, closed). |
ACTION |
The action to be taken by the operation (e.g., open, close). |
PHASES |
The phase(s) to be operated by the step. |