Add a Domain to the Geodatabase

  1. Right-click the name of the geodatabase and select Properties.
  2. Click the Domains tab.
  3. Scroll to the bottom of the domains list.
  4. In the empty row, type the domain name in the Domain Name field.
  5. Ensure that the correct Field Type is selected under Domain Properties.
  6. If additional domains need included, click Apply after adding each one.
  7. Click OK.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?