Fiber Lambda
Properties:
-
Field Type: Double
-
Domain Type: Coded Values
-
Split Policy: Duplicate
-
Merge Policy: Default Value
Coded Values:
Code |
Description |
---|---|
850 |
850 nm |
1310 |
1310 nm |
1470 |
1470 nm |
1490 |
1490 nm |
1510 |
1510 nm |
1550 |
1550 nm |
1570 |
1570 nm |
1590 |
1590 nm |
1610 |
1610 nm |