Configure Data

Both circuit and splice schematics require the SchematicExportAttribute model name be assigned in the geodatabase to identify necessary attributes. If you're performing both optional configurations (for splice and circuit schematics), you only need to complete this process once.

TIP: Data are displayed using the ArcFM Primary Display Field. The Primary Display Field is set on the Field Display tab of the ArcFM Properties Manager.

For the classic fiber features, assign this model name as shown below. If you want additional attributes in your schematics, you will need to assign the SchematicExportAttribute model name to those attributes as well.

IMPORTANT: When you assign the SchematicExportAttribute model name to a new field, you will need to edit the field's storage mode in ArcCatalog's Schematics Dataset Editor. See the help topic SchematicExportAttribute Model Name for more information.

DevicePoint

Field Model Names:

Field

Field Model Name

LocationDescription

SchematicExportAttribute

FiberOpticCable

Field Model Names:

Field

Field Model Name

CableName

SchematicExportAttribute

PatchLocation

Field Model Names:

Field

Field Model Name

Name

SchematicExportAttribute

F_BacksidePort

Field Model Names:

Field

Field Model Name

PortName

SchematicExportAttribute

F_BufferTube

Field Model Names:

Field

Field Model Name

BufferTubeNumber

SchematicExportAttribute

BufferTubeColor

SchematicExportAttribute

BufferTubeName

SchematicExportAttribute

F_Device

Field Model Names:

Field

Field Model Name

Name

SchematicExportAttribute

F_Fiber

Field Model Names:

Field

Field Model Name

FiberNumber

SchematicExportAttribute

FiberColor

SchematicExportAttribute

FiberName

SchematicExportAttribute

F_FrontsidePort

Field Model Names:

Field

Field Model Name

PortName

SchematicExportAttribute

F_PatchPanel

Field Model Names:

Field

Field Model Name

Name

SchematicExportAttribute

F_Rack

Field Model Names:

Field

Field Model Name

Name (suggested field)

SchematicExportAttribute

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?