Configure Data
Both circuit and splice schematics require the SchematicExportAttribute model name be assigned in the geodatabase to identify necessary attributes. If you're performing both optional configurations (for splice and circuit schematics), you only need to complete this process once.
For the classic fiber features, assign this model name as shown below. If you want additional attributes in your schematics, you will need to assign the SchematicExportAttribute model name to those attributes as well.
DevicePoint
Field Model Names:
Field |
Field Model Name |
---|---|
LocationDescription |
SchematicExportAttribute |
FiberOpticCable
Field Model Names:
Field |
Field Model Name |
---|---|
CableName |
SchematicExportAttribute |
PatchLocation
Field Model Names:
Field |
Field Model Name |
---|---|
Name |
SchematicExportAttribute |
F_BacksidePort
Field Model Names:
Field |
Field Model Name |
---|---|
PortName |
SchematicExportAttribute |
F_BufferTube
Field Model Names:
Field |
Field Model Name |
---|---|
BufferTubeNumber |
SchematicExportAttribute |
BufferTubeColor |
SchematicExportAttribute |
BufferTubeName |
SchematicExportAttribute |
F_Device
Field Model Names:
Field |
Field Model Name |
---|---|
Name |
SchematicExportAttribute |
F_Fiber
Field Model Names:
Field |
Field Model Name |
---|---|
FiberNumber |
SchematicExportAttribute |
FiberColor |
SchematicExportAttribute |
FiberName |
SchematicExportAttribute |
F_FrontsidePort
Field Model Names:
Field |
Field Model Name |
---|---|
PortName |
SchematicExportAttribute |
F_PatchPanel
Field Model Names:
Field |
Field Model Name |
---|---|
Name |
SchematicExportAttribute |
F_Rack
Field Model Names:
Field |
Field Model Name |
---|---|
Name (suggested field) |
SchematicExportAttribute |