Fiber Overhead Underground
-
This domain is not required but it tells the glass report into which category to put a particular cable’s glass length. These values don’t have to be stored in a domain, but doing so means less typing for users.
-
Overhead and Underground coded values should always be included in this domain. Other values are optional.
Properties:
-
Field Type: Text
-
Domain Type: Coded Values
-
Split Policy: Duplicate
-
Merge Policy: Default Value
Coded Values:
Code |
Description |
---|---|
Bridge |
Bridge |
Direct Buried |
Direct Buried |
Overhead |
Overhead |
Underground |
Underground |