Fiber Tray Number

TIP: This field is not required but if you use this domain, Fiber Manager uses the tray numbers you provide under Coded Values. Otherwise, hardcoded tray numbers 1 through 15 are used.

Properties:

  • Field Type: Integer

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

1

1

2

2

3

3

4

4

5

5

6

6

7

7

8

8

9

9

10

10

11

11

12

12

13

13

14

14

15

15

16

16

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?