Fiber Active Device Type

Active devices are those that are powered, while passive devices are not powered. Those two concepts are important in the world of WDM (wavelength division multiplexing).

TIP: This domain is not required, and the values provided are just examples. If you include this domain, the coded values should contain items from your inventory.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

Back Plate

Back Plate

CATV Fiber Node

CATV Fiber Node

CCTV

CCTV

DWDM

DWDM

JMUX

JMUX

Jumper

Jumper

Media Converter

Media Converter

Micronode

Micronode

Microwave

Microwave

ONU

ONU

Optical Amplifier

Optical Amplifier

OTDR Remote Terminal

OTDR Remote Terminal

Power Supply

Power Supply

Proactive Relay

Proactive Relay

Receiver

Receiver

RFAmplifier

RFAmplifier

Router

Router

SONET

SONET

Switch

Switch

Telemetry

Telemetry

Telephony Switch

Telephony Switch

Terminator

Terminator

Transmitter

Transmitter

Transport

Transport

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?