Create Domains

Two domains are added when you run the Upgrade ArcFM Solution Database tool in ArcCatalog:

  • Fiber Field Model Name

  • Fiber Object Model Name

In addition to the domains above, you should never modify the names and values of the following domains:

  • Fiber Availability Indicator

  • Fiber Mode

  • Fiber Optic Cable Length Source

  • Fiber Overhead Underground

  • Fiber Units of Measure

  • SpliceType

  • Yes / No

Keep in mind that the field type of a domain must match the data type of a field to which it is assigned.

Visit this page for information about adding a domain to the geodatabase.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?