Fiber Fault Subtype

TIP: This field is not required but is used in conjunction with Fiber Fault Status.

Properties:

  • Field Type: Integer

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

0

Animal

1

Dig In

2

Fire

3

Gunshot

4

Internal

5

Storm

6

Tree

7

Vandal

8

Vehicle

9

Other

10

Unknown

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?