Set Snapping Properties
This is an optional step but recommended. You can use the ArcFM Snapping Manager to establish snapping properties for Fiber Manager feature classes. The following table uses sample data as a guide in establishing the snapping order and snapping targets. When snapping to more than one feature class, the snapping order corresponds to the top to bottom order as listed in the table.
Feature Class |
Snaps to Feature Class |
Vertex |
Edge |
End |
---|---|---|---|---|
DevicePoint |
FiberOpticCable |
X |
||
FiberFault |
FiberOpticCable |
X |
X |
|
FiberOpticCable |
DevicePoint |
X |
X |
|
PatchLocation |
X |
X |
||
SplicePoint |
X |
X |
X |
|
SplitterLocation |
X |
X |
||
FiberSlackLoop |
FiberOpticCable |
X |
X |
|
FiberStructure |
ConduitSystem |
X |
X |
|
PatchLocation |
FiberOpticCable |
X |
||
SplicePoint |
FiberOpticCable |
X |
X |
X |
SplitterLocation |
FiberOpticCable |
X |
X |
|
TransitionPoint (including Riser andDemarcation Point subtypes) |
FiberOpticCable |
X |
X |