Fiber Splice Location Type

TIP: This domain is not required, but you can use it to track splice location types, which would make future queries easier.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

Handhole

Handhole

Pedestal

Pedestal

Pole Mounted

Pole Mounted

Span Mounted

Span Mounted

Vault

Vault

Other

Other

Unknown

Unknown

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?