Export XML

This step is optional but highly recommended. Use the XML Import/Export tool to export your geodatabase into an XML file. Export all properties available in the ArcFM XML Export tool. Keep this file as a backup. If necessary, you can also use the XML Import/Export tool to import this file into your geodatabase.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?