Fiber Parent Type

TIP: This domain is not required, but as discussed in Relationship Advice, the model names contained below are required for the relationships to understand the parent/child connections. This domain is recommended for convenience. When building relationships, selecting from a short list of parent types is easier than selecting from the entire list of model names.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

ACTIVEDEVICE

ACTIVEDEVICE

FIBERPATCHLOCATION

FIBERPATCHLOCATION

PASSIVEDEVICE

PASSIVEDEVICE

RACK

RACK

RFNODE

RFNODE

SHELF

SHELF

SPLICEPOINT

SPLICEPOINT

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?