Welcome

Welcome to the Fiber Manager Configuration Guide. Here are some tips to help you find relevant information fast:

  • Topics are organized thematically in the Table of Contents along the left-hand side.

  • Click the arrow icon to expand topics and reveal subtopics.

  • Use the Search field to type keywords you’re looking for. The Search queries our entire catalog of guides, and further, it allows you to filter by product, guide type, and version. Enter your search terms to get started.

  • While reading a topic, press the down key to scroll down through the topic, and press the right key to move to the next topic.

  • Use the, “Was this helpful?” feedback options to drop us a note! Your comments help us improve documentation so you can get your job done most effectively.


What’s the user community searching for? Here are the top five topics from the last six months:

  1. Fiber Manager Data Architecture Overview

    1. This is a great place to get started to learn about the Fiber Manager data model.

  2. Create Fiber Favorites

    1. Favorites are pre-saved fiber assets ready for end users to sketch on the map. Building them is a critical and required component of the application, and this topic gets you started on the right foot.

  3. Create and Configure Tables

    1. Fiber Manager uses object tables to track most of the fiber assets. Start here to learn more about each related table.

  4. F_SPLITTER

    1. This particular table topic is likely getting a lot of recent attention due to Wavepoint now supporting splitters. Check this topic out to learn the difference between F_SPLITTER and F_SPLITTERDEVICE.

  5. Wavepoint Rack View Configuration

    1. The decisions you make while configuring Fiber Manager could have an effect on how assets are displayed in Wavepoint . Start at this topic to understand these decisions. Also, Wavepoint has its own comprehensive configuration guide. Please see the Wavepoint Configuration Guide for more information.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?