Fiber Device Subtype

TIP: This domain is not required although it’s used in conjunction with Fiber Device Type.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

0

CATV Device

1

CATV Fiber Node

2

CCTV

3

Cell Tower Receiver

4

Demultiplexor

5

DWDM

6

JMUX

7

Media Converter

8

Metering

9

Microwave

10

Multiplexor

11

NIU

12

OLT

13

ONU

14

OTDR Remote Terminal

15

Proactive Relay

16

Protective Relay

17

Router

18

SCADA

19

SONET

20

Substation Automation

21

Switch

22

Telemetry

23

Telephony Switch

24

Other

25

Unknown

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?