SpliceType

IMPORTANT: This domain is not required but it provides the values in the Splice Type field in Fiber User Settings, Fiber System Settings, and Connection Manager. This domain must be spelled and capitalized exactly as shown. If this domain already exists in the geodatabase, it must NOT be renamed in any way.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

TIP: Coded Values — We strongly encourage you to include Continuous, Fusion, and Jumper.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?