Settings for Features with Color

These settings apply to any feature or object classes.

Any feature or object in the fiber data set can use color. For example, the F_FIBER and F_BUFFERTUBE tables use color to identify strands and the tubes containing them.

TIP: Using this table
  • The Example Field Name, Data Type, and Domain columns contain values entered while creating the feature. If using the worksheet, record these values in Table 5.

  • The Assign Field Model Name column contains a value entered in the ArcFM Properties Manager dialog, Field Model Names tab. If using the worksheet, record these values in Table 5.

Function

Settings

 

Example Field

Data Type

Domain

Assign Field Model Name

Features that have color

FiberColoredField

Text

Fiber Colors

FIBERCOLOREDFIELD

FiberColorNameField

Text

Fiber Color Names

FIBERCOLORNAMEFIELD

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?