Fiber Mode
-
This domain is not required but modetype functionality and counting ability in Fiber Manager need a field with these particular values.
-
Coded values other than the ones below are not supported.
-
These values don’t have to be stored in a domain, but doing so means less typing for users.
Properties:
-
Field Type: Text
-
Domain Type: Coded Values
-
Split Policy: Duplicate
-
Merge Policy: Default Value
Coded Values:
Code |
Description |
---|---|
Multimode |
Multimode |
Singlemode |
Singlemode |