Fiber Rack Location

TIP: This domain is not required, but you can use it to track rack location in the patch location

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

Aisle

Aisle

Bay

Bay

Floor Mounted

Floor Mounted

Free Standing

Free Standing

Pad Mounted

Pad Mounted

Wall Mounted

Wall Mounted

Other

Other

Unknown

Unknown

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?