Fiber Circuit Name

TIP: This domain is not required but allows you to assign names to circuits. The Coded Values below are just examples.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

Distribution Automation

Distribution Automation

Interoffice

Interoffice

Substation

Substation

Other

Other

Unknown

Unknown

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?