Flexible Patch Panel Connection Report
Configure either the Flexible Patch Panel Connection Report OR the Original Patch Panel Connection Report.
This report must be used with flexible features. However, you may wish to use this report on existing (standard or classic) features. To do this you must perform the configuration. The previous Patch Panel Connection Report will not continue to work after the upgrade steps to use the Flexible Patch Panel Connection Report. The configuration outlined below is optional.
Add Fields
When discussing parent, child and first parent objects, this example will use the following hierarchy (top to bottom). The First Parent is the object that contains the object with the FiberDataTableSource model name assigned. Identify the feature to which this model name is assigned (e.g., F_PatchPanel), then identify the feature that contains it (e.g., F_Rack). In this section, we'll refer to this feature as the First Parent because other features may also be parents, but this one is unique.
-
PatchLocation
-
F_Rack
-
F_PatchPanel (has FiberDataTableSource model name assigned)
-
F_PatchPanelCard
-
F_BacksidePort and F_FrontsidePort (both have relationships to F_PatchPanelCard)
TIP: The tables at the bottom of this page show the fields that must be added, their data types and whether they require a default value. DO NOT assign model names until you've completed all other steps first.
- First you will need to identify the objects that appear in the Patch Panel Connection report. To do this, you may want to run this report and make note of the features and objects that appear on it.
-
In ArcCatalog, add the following fields to any object that
acts as a parent (or first parent) for other objects. For example,
Patch Location, F_Rack, F_PatchPanel, F_PatchPanelCard. Assign a default
value to each field.
-
FiberGridDefaultWidth (long integer)
-
FiberGridDefaultHeight (long integer)
-
FiberNumberGridRows (long integer)
-
FiberNumberGridColumn (long integer)
-
- Add the FiberFacetsContained (text data type) field to the first parent. In our example, this would be the F_Rack object. Assign a default value to this field.
-
Next, add the following fields to any object that acts
as a child to other objects. For example, F_Rack, F_PatchPanel, F_PatchPanelCard,
F_BacksidePort, F_FrontsidePort. Assign a default value to each field.
-
FiberGridDefaultWidth (long integer)
-
FiberGridDefaultHeight (long integer)
-
FiberGridPosition (long integer)
-
-
Add the FiberFacetsContainedBy (text data type) field to
the child of the first parent. In our example, this would be the F_PatchPanel,
F_PatchPanelCard, F_BacksidePort, F_FrontsidePort objects. Assign
a default value to this field.
Add Default Values to Existing Features
In the next few steps, you'll assign default values to the existing features. The default values assigned in previous steps will apply to newly placed features.
-
Open the geodatabase in ArcMap.
-
Ensure the features and objects to which you added fields are included in the map. They should be visible on the List by Source tab.
-
Start an editing session.
-
On the List by Source tab, select an object to which you added a field with a default value. Right-click the object and select Open. This displays the Attributes window.
-
Locate the column (field) to be updated. Right-click it and select Field Calculator. The Field Calculator will be disabled if you do not have an editing session started.
-
In the field at the bottom of the window, enter the default value to which you want to set this field on all objects in the map. If you're entering a numeric value, just enter the value (see image below). If you're entering an alpha-numeric value, use quotes (e.g., "FB").
-
Click OK to assign the default values to the fields.
-
Repeat these steps for all fields with default values on all feature or object classes to which you added them.
-
Don't forget to assign a value to the FiberGridPosition field in ArcMap. If this field is <Null> you will receive errors when attempting to display the Patch Panel Connection Report.
Add Model Names to Domains
The following model names are used by the Flexible Patch Panel Connection report and must be added to the appropriate domains:
Fiber Object Class Model Name
FiberGridableContainer
FiberGridableObject
FiberFacetedObject
ReverseOrderChildren
PatchLocationReportable
Fiber Field Model Name
FiberFacetsContained
FiberFacetsContainedBy
FiberGridDefaultHeight
FiberGridDefaultWidth
FiberGridPosition
FiberNumberGridRows
FiberNumberGridColumns
-
Assign Model Names
If you're upgrading an existing geodatabase to use the new Patch Panel Connection Report on existing (originated in the static model) features, make note of the features you need to modify. Assign the fields, model names and field model names as outlined below. Make note of any default values you assign. You must update existing features in the geodatabase to reflect the default values set while creating the new fields below.
Add the following field names to features and objects you want to appear in the Patch Panel Report. The settings depend on whether the feature you're configuring is a parent or a child or both.
-
The Example Field Name and Data Type columns contain values entered when the feature is created. If using the worksheet, record these values in Table 5.
-
The Field Model Name column contains values entered in the ArcFM Properties Manager on the Field Model Names tab. If using the worksheet, record these values in Table 5.
Parent Features
The parent objects (F_Rack, F_PatchPanel, F_PatchPanelCard) require the following model names in order to appear in the Patch Panel Connection report. Record these model names in Tables 4 (Class) and 5 (Field) of the worksheet for your custom parent features.
|
Function |
Settings |
|||
|---|---|---|---|---|
|
Example Field Name |
Data Type |
Field Model Name |
Class Model Name |
|
|
Include in Patch Panel Report (Parent objects) |
FIBERGRIDABLECONTAINER |
|||
|
FiberGridDefaultWidth* assign a default value; the value you assign depends on the format |
Long Integer |
FIBERGRIDDEFAULTWIDTH |
||
|
FiberGridDefaultHeight* assign a default value; the value you assign depends on the format |
Long Integer |
FIBERGRIDDEFAULTHEIGHT |
||
|
FiberNumberGridRows** assign a default value |
Long Integer |
FIBERNUMBERGRIDROWS |
||
|
FiberNumberGridColumns** assign a default value |
Long Integer |
FIBERNUMBERGRIDCOLUMNS |
||
Assign the REVERSEORDERCHILDREN class model name to your rack table if you want the item in position 1 to appear at the bottom of the rack instead of the top within patch panel connection reports.
* The FiberGridDefaultWidth and FiberGridDefaultHeight fields must have default values assigned to them when the fields are created. These values determine the amount of space allotted on the report for empty fields or values with no label text. The fields use units the size of one spacebar space in Internet Explorer in the language set on the computer.
**The FiberNumberGridRows and FiberNumberGridColumns fields must also be assigned default values when they're created. These fields indicate the number of rows or columns in the object.
Child Features
Next, determine which objects are child features (features that are contained by another). In the example given above, F_Rack is the First Parent and cannot be a child object in this case. In the above example, F_PatchPanel, F_PatchPanelCard, F_BacksidePort, and F_FrontsidePort are the child objects. These are all contained by a parent.
-
The Example Field Name and Data Type columns contain values entered when the feature is created. If using the worksheet, record these values in Table 5.
-
The Field Model Name column contains values entered in the ArcFM Properties Manager on the Field Model Names tab. If using the worksheet, record these values in Table 5.
Child objects require the following model names. Record these model names in Tables 4 (Class) and 5 (Field) of the worksheet for your custom child objects.
|
Function |
Settings |
|||
|---|---|---|---|---|
|
Example Field Name |
Data Type |
Field Model Name |
Class Model Name |
|
|
Include in Patch Panel Report (Child objects) |
FIBERGRIDABLEOBJECT |
|||
|
FiberGridDefaultWidth* assign a default value; the value you assign depends on the format |
Long Integer |
FIBERGRIDDEFAULTWIDTH |
||
|
FiberGridDefaultHeight* assign a default value; the value you assign depends on the format |
Long Integer |
FIBERGRIDDEFAULTHEIGHT |
||
|
FiberGridPosition** This field contains the position of the feature in the grid. This is not generally set using a default value, but every placed feature MUST have a value in this field. If this field is <Null>, errors will occur when you attempt to run the Patch Panel Connection Report. |
Long Integer |
FIBERGRIDPOSITION |
||
* The FiberGridDefaultWidth and FiberGridDefaultHeight fields must have default values assigned to them when the fields are created. These values determine the amount of space allotted on the report for empty fields or values with no label text. These fields use units the size of one spacebar space in Internet Explorer in the language set on the computer (e.g., English, Spanish, etc.).
**The grid position goes from left to right, top to bottom. The upper left corner is position 1.
First Parent
The Patch Panel Connection Report will display multi-sided objects and the objects connected to those sides. Even if the First Parent (e.g., F_Rack) has only one side, you must still assign the model name and set the value to indicate that side (e.g., F for front). If you skip this step, you will get errors when attempting to run the report.
The First Parent requires the following model names:
|
Function |
Settings |
|||
|---|---|---|---|---|
|
Example Field Name |
Data Type |
Field Model Name |
Class Model Name |
|
|
Include Faceted Object in Patch Panel Report |
FIBERFACETEDOBJECT |
|||
|
FiberFacetsContained Assign a default value. This field indicates the designations for the sides of the objects (e.g., F_Rack has two sides: F and B. So the default value in this field might be FB). |
Text |
FIBERFACETSCONTAINED |
||
Children of First Parent
All children of the First Parent require the following field and field model name. In the example we've been using this means the following objects: F_PatchPanel, F_PatchPanelCard, F_BacksidePort and F_FrontsidePort.
|
Function |
Settings |
|||
|---|---|---|---|---|
|
Example Field Name |
Data Type |
Field Model Name |
||
|
Include Faceted Objectd in Patch Panel Report |
FiberFacetsContainedBy* |
Text |
FIBERFACETSCONTAINEDBY |
|
*The field with the FiberFacetsContainedBy model name indicates to which side of the parent object this object connects (e.g., F or B). So (using the previous example) because both sides of F_Rack contain both F_PatchPanel and F_PatchPanelCard, the default values for this field on these two objects would be FB. F_PatchPanelCard contains two different objects: F_BacksidePort and F_FrontsidePort. In this example F_FrontsidePort connects to side F, making the FiberFacetsContainedBy field default value on the F_FrontsidePort object F. F_BacksidePort connects to side B, making the FiberFacetsContainedBy field default value on the F_BacksidePort object B.
Even if the parent object has only one facet, the field must still exist and indicate to which facet on the parent the child connects.