Fiber Connection Type

TIP: This domain is not required but helps differentiate between fiber optic and electronic connections.

Properties:

  • Field Type: Integer

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

1

Fiber Optic

2

Electronic

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?