F_FIBER

IMPORTANT:
  • ObjectID fields are automatically created (by Esri) when you create the schema.

  • GlobalID fields are required by Fiber Manager and are created with Esri's Add Global ID tool (Manage > Add Global IDs).

  • Tables must be versioned for an SDE database. See Esri’s documentation for more information about versioning tables.

  • Tables must also be converted to ArcFM Objects.

  • In ArcGIS applications, there are four numeric data types: Short Integer, Long Integer, Float, and Double. The choices reflect a balance between minimizing storage space while still allowing enough range and precision for the field to be useful. For example, because lengths typically have decimals, these fields are assigned either Float or Double.

    In the table below, any field set to integer does need to be either a Short or Long Integer, as these fields cannot contain decimals. So, the decision comes down to the minimum and maximum values you need for the field:

    • Short Integer Storable Range: -32,768 to 32,767

    • Long Integer Storable Range: -2,147,483,648 to 2,147,483,647

    So, as an example, would you ever have more than 32,767 patch panels on a single rack? No. So, the RackPosition field could be a Short Integer. Conversely, foot or meter stamps along a cable could easily exceed 32,767. So, CableMarking fields should be a Long Integer. Our integer recommendations err on the side of more range and usefulness, but your company could decide to change a Long Integer to a Short Integer (or a Double down to a Float) if you knew the maximum values would never exceed the types’ upper threshold.

Alias: Strand

TIP: You can change the length of Text fields to a number that is appropriate for your organization.

Field

Data Type

Default Value

Domain

Length/Precision

Available

Short Integer

 

Fiber Availability Indicator

 

FiberChildClassModelName

Alias: Fiber Child Class Model Name

Text

   

50

FiberColor

Alias: Color

Text

 

Fiber Colors

50

FiberName

Name

Text

 

Fiber Color Names

50

FiberNumber

Number

Long Integer

     

FiberParent

Alias: Fiber Parent

Guid

     

FiberParentClassModelName

Alias: Fiber Parent Class Model Name

Text

   

50

ModeType

Alias: Mode

Text

 

Fiber Mode

50

Status

Text

 

Fiber Status

50

ThisFiberClassModelName

Alias: This Fiber Class Model Name

Text

FiberStrand

 

50

Field Display

Primary Display Field: Choose this field in the ArcFM Properties Manager. The chosen field is displayed when using ArcFM tools such as the ArcFM Locator and ArcFM Attribute Editor. Your company can choose the most useful field to display for the end users. If the chosen field is null for the selected or identified features, the display field defaults to the ObjectID.

Display Name Object: Fiber Namer, which is an out-of-the-box naming function that combines the Strand Number and Strand Color. If selected, it does not incorporate what is chosen in the Primary Display Field. If left null, the application will use what is in the Primary Display Field.

Model Names

FIBERCONNECTABLEOBJECT, FIBEROBJECT, FIBERSTRAND, SUPPORTSALOSS, SUPPORTSBLOSS, SUPPORTSCONNECTIONTYPE, SUPPORSTRAYS

Field Model Names

Available: AVAILABLE, FIBERALLOCATIONREPORTFIELD, FIBERSPLICEREPORTFIELD

GlobalID: GLOBALID

FiberChildClassModelName: FIBERCHILDCLASSMODELNAME

FiberColor: FIBERSTRANDCOLOR, FIBERCOLOREDFIELD,

FiberName: FIBERSTRANDCOLORNAME, FIBERSTRANDNAME, FIBERCOLORNAMEFIELD, SCHEMATICEXPORTATTRIBUTE

FiberNumber: FIBERSTRANDNUMBER, FIBERCONNECTIONDISPLAYSORTFIELD

FiberParent: FIBERPARENT

FiberParentClassModelName: FIBERPARENTCLASSMODELNAME

ModeType: MODETYPE

Status: FIBERSTATUS

ThisFiberClassModelName: THISFIBERCLASSMODELNAME

Object AutoUpdaters

On Feature Delete: ArcFM Fiber Object Deleted

Field Autoupdaters

Available — On Feature Update: ArcFM Fiber Availability

ChangeDate — On Feature Update: ArcFM Current Date

ChangeUser — On Feature Update: ArcFM Login User Name

CreationDate — On Feature Create: ArcFM Current Date

CreationUser — On Feature Create: ArcFM Login User Name

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?