Fiber Color Names

TIP: Although this domain is not required, it uses color abbreviations to minimize column width in various reports and helps make populating Favorites faster.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

BL

BL

OR

OR

GR

GR

BR

BR

SL

SL

WH

WH

RD

RD

BK

BK

YL

YL

VL

VL

RS

RS

AQ

AQ

BL1

BL1

OR1

OR1

GR1

GR1

BR1

BR1

SL1

SL1

WH1

WH1

RD1

RD1

BK1

BK1

YL1

YL1

VL1

VL1

RS1

RS1

AQ1

AQ1

BL2

BL2

OR2

OR2

GR2

GR2

BR2

BR2

SL2

SL2

WH2

WH2

RD2

RD2

BK2

BK2

YL2

YL2

VL2

VL2

RS2

RS2

AQ2

AQ2

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?