Create and Manage Fiber Favorites

Fiber assets have an abundance of relationships and attributes. It would be untenable for Fiber Editors to have to create fiber assets from scratch every time they needed to sketch one.

Fiber favorites are pre-attributed, pre-related, and pre-saved fiber assets, ready for Fiber Editors to grab and get to work. They are a required part of any Fiber Manager XI implementation, and they are key to the long term success of the application at your company.

Creating and managing fiber favorites occurs on the left-hand side of Fiber Builder (favorites vary by company, so your favorite categories differ from the following image).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?