BQT6904400-03

Performing the Cable Test

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
  • Ensure the test process & procedure as per latest IEC 62271-200.
  • Apply appropriate PPE and follow safe work practices.
  • This equipment must only be tested by qualified personnel.
  • Make sure that the metallic components of the test adapter are at a sufficient distance from the earthed switchgear components (for example, housing).
Failure to follow these instructions will result in death or serious injury.
NOTE: Make sure that the metallic components of the test adapter are at a sufficient distance from the earthed switchgear components (for example, housing).
  1. Connect the test adapter to a free cable connection in the cubicle and on the test unit. To this effect, observe the specifications of the test unit’s manufacturer.

  2. Set switchgear cubicle to test position:

    Table 18 Performing the Cable Test

    Component

    Test position

    VCB OFF
    Trolley In disconnected position
    Earthing switch OFF
    NOTE: While performing cable test, comply with the admissible limits (see Table 19).
  3. Perform cable test according to the cable manufacturer’s specifications.

Reposition the cable connection in the cable compartment:

  1. Earth I/F cable again.

  2. Remove test set.

  3. Reconnect VT and surge arrester or de-earth them.

  4. Reposition cable compartment cover.

Admissible Limits for the Cable Test in Cubicles

Table 19 Admissible Limits for the Cable

 

DC test voltage [kV] max.
15 min.

AC – VLF test voltage

(0.1 Hz) 60 min.

MCSeT (Ur = 24 kV)

48 kV(1)(2)

36 kV(1)(2)

72 kV(3)

54 kV(3)

(1) Category A: This category comprises those systems in which any phase conductor that comes in contact with earth or an earth conductor is disconnected from the system within 1 min.

(2) Category B: This category comprises those systems which under fault conditions are operated for a short time with one phase earthed. This period according to IEC 60183, should not exceed 1 h. For cables covered by this standard, a longer period not exceeding 8 h on any occasion can be tolerated. The total duration of earth faults in any year should not exceed 125 h.

(3) Category C: This category comprises all systems which do not fall into category A or B.

NOTE: A DC test may endanger the insulation system under test. Where possible an AC test should be used as described above.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?