BQT6904400-04

Installing the Surge Arresters

CAUTION
hazard of inappropriate assembly
Ensure to remove the surge arrester assembly in order to access the cable compartment from the front.
Failure to follow these instructions can result in injury or equipment damage.

Follow the below steps to assemble the surge arrester:

  1. Install the surge arrester (3) to the support channel (1) with a U nut (2)

    (Figure 81).

  2. Connect the surge arrester terminal (4) to the Fixed VT connection copper

    bar (5).

  3. Insert the plastic bolt (8) along with screw (6) , washer (7) and nut (9).

  4. Install the insulation cover (10).

  5. For standard torque values, refer to Standard Tightening Torques and comply with the specified torque values.

Figure 81
Installing the Surge Arresters

1

Support channel

6

Screw M8 x 20

2

U nut

7

Washer M8

3

Surge arrester

8

Plastic bolt

4

Surge arrester terminal

9

Nut M8

5

Fixed VT connection copper bar

10

Insulation cover

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.