BQT6904400-03

Surface Condition

NOTICE
HAZARD OF INCORRECT EQUIPMENT OPERATION
  • Before positioning the switchgear at its installation site, ensure that the fastening points are at the correct level.
  • Unevenness must not exceed ± 2 mm/m and there must not be a height difference of more than 6 mm over the entire width of the switchgear.
Failure to follow these instructions can result in equipment damage.

Laser check is required for accurate check of the floor levelness. Floor level is more essential for correct assembly and performance of the product.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?