BQT6904400-03

Preparation of Cable Compartment

Access the cable compartment. Refer to Access to the Cable Compartment, User Guide (BQT6904800).

  1. Release the cable clamp hardware screw (1), washer (2), and nut (5).

  2. Remove the top cable clamp (6) and bottom cable clamp (4).

  3. Remove the gland plate neck ring (3).

  4. Remove base plate (7) as required.


Figure 66
Preparation of Cable Compartment

1

Screw M10 x 90

5

Nut M10

2

Washer M10

6

Top cable clamp

3

Gland plate neck ring Ø72

7

Base plate

4

Bottom cable clamp

   
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?