BQT6904400-03

Cable Test after Assembly (Optional)

WARNING
hazard of incorrect operation
Comply with the Safety Provisions.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

A test unit and a test adapter (not included in scope of supply) are required for cable testing.

NOTE: The assembly, operating and testing instructions for cable fittings and connectors and the test unit must be taken into consideration.

During the cable test, the busbar can be operated at rated voltage (see Rating Plate). For qualification of the current transformers for cable tests, enquire at the appropriate manufacture.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?