BQT6904400-03

Control Symbols of E/S

Table 12 Control Symbols of E/S

Description

Symbol

Description

Symbol

Operation position

Closed E/S mechanical indicator

Open E/S mechanical indicator

Position can be locked using pad lock

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?