BQT6904400-04

Ground Plan of a MCSeT Switchgear within a Switchgear Room

Figure 17
Dimensions in the Switchgear Room

1

C-channel rail

3

Opening for routing high-voltage cables

2

Opening for routing external low-voltage cables

4

Power cable trench

Cubicle width A (mm)

Dimension B (mm)

Rated voltage
7.2 kV

Rated voltage

12/17.5 kV

Rated voltage
24 kV

400

285

650

400

800

550

550

1000

750

750

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.