BQT6904400-03

Control Symbols of VCB

Table 13 Control Symbols of Rack-In/Rack-Out

Description

Symbols

Manual operation instruction for rack-in/rack-out

Connected/service position

Disconnected/test position

Table 14 Control Symbols of EvoPacT HVX VCB

Description

Symbol

Description

Symbol

ON push button

Spring discharged

OFF push button

Operating counter

Spring charged and ready-to-close indicator

Position selector lockable with padlocking

VCB OFF

VCB ON

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?