Handling Instructions
WARNING |
|---|
|
HAZARD OF EQUIPMENT TOPPLING
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The transport and handling information of cubicle are as follows:
-
The conditions and types of transport have been stipulated in the contract details.
-
The type of packaging depends on the type of transport and the storage conditions.
-
The cubicles are delivered individually and are fastened on pallets. The standard accessories are included.
-
The transport trolley with accessories will be dispatched in a separate box.
-
The VCB rated above 2500 A will be dispatched in a separate package.
-
The cubicles are delivered in vertical position.
-
The weight of the entire transport unit is indicated on the packaging.
Packaging
| NOTICE |
|---|
|
Hazard of incorrect handling
Failure to follow these instructions can result in equipment damage.
|
The packaging for various modes of transportation are as follows:
-
If packed exclusively for truck transport, the cubicles are delivered on a pallet with PE protective film (Figure 8).
-
For sea transport, the units are packed in sealed aluminium foil with desiccant and in a closed wooden case with tightly closed wooden base (also for container transport, see Figure 9).
-
In case of air transport, the cubicles are packed in wooden crates with a protective PE film hood (dust protection) or in wooden crates, also with closed wooden bases, however without protective hoods.
WARNING