BQT6904400-03

Detailed View of Bottom Plates

Figure 18
Bottom Plate of 400 mm Feeder with Contactor Cubicle

Figure 19
Bottom Plate of 650 mm Cubicle with Four Runs

Figure 20
Bottom Plate of 650 mm Cubicle with Two Runs

Figure 21
Bottom Plate of 800 mm Cubicle for 12/17.5 kV

Figure 22
Bottom Plate of 800 mm Cubicle for 24 kV

Figure 23
Bottom Plate of 1000 mm Cubicle for 12/17.5 kV

Figure 24
Bottom Plate of 1000 mm Cubicle for 24 kV

Figure 25
Bottom Plate of 800 mm Top Busway Entry Cubicle 24 kV

Figure 26
Bottom Plate of 1000 mm Top Busway Entry Cubicle 24 kV

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?